cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.18 / STM32F7 package 1.5.1

Mark Skeete
Associate II
Posted on January 03, 2017 at 18:47

Hi All,

Are the 64pin versions of the stm32f7 chips in cubeMX?

I can find the 100 pin parts but not the 64 pin parts

Mark

#stm32f7 #stm32cubemx
5 REPLIES 5
Nesrine M_O
Lead II
stm32cube-t
Senior III
Posted on January 16, 2017 at 10:24

Dear user,

Here are the supported STM32F7MCUs  in LQFP100 package in CubeMX 4.19 (out this week). This is aligned with the Datasheet. Can you confirm you find the MCU you need?

0690X000006063CQAQ.png
Mark Skeete
Associate II
Posted on January 16, 2017 at 17:47

Hi

I'm looking for the 64 pin package.

Specifically, the STM32F723ZE as I think thats the only F7, 64 pin part at the moment
Jeanne Joly
Senior III
Posted on January 23, 2017 at 11:09

Hi Mark Skeete,

Please upgrade the CubeMX release to 4.19.

You will have 3 MCUs with 64 pin : 

0690X000006066dQAA.png

You can see them on ST website as well : 

0690X000006066TQAQ.png

BR

Eric

Posted on January 23, 2017 at 12:03

Thank you.

I updated a few days ago and saw them