2022-04-06 5:47 PM
I'm using STM32CUBEIDE with macOS.
I do not know why I cannot click the button there.
Are there any solutions for this issue?
There is no this kind of problem in the Windows system.
Thanks
2022-04-14 3:33 AM
Hello @FWu.3 ,
Do you have still this problem to solve?
If yes, please precise which CubeMX version used.
This is a problem with CubeMx tool (not CubeIDE).
Imen
2022-05-30 9:03 AM
I also have this issue. The STM32CubeMX Eclipse IDE feature (the plugins are STM32CubeMX and STM32CubeMX Integration Utilities) has version 6.5.0-RC4, build 20220225-1913 (UTC). Is there any workaround?
Best,
Pietro
2022-06-22 10:23 AM
Hello,
I'm having the very same issue with CubeIDE v 1.9.0 (CubeMx v 6.5.0 RC4) on macOS.
Is there already a solution for this? It's quite annoying
Thanks
Andrea