2018-09-18 9:08 PM
I use STM32Cube Ver 4.26.1 to generate LWIP code with HTTPD, it keep print "Assertion "HTTP headers not included in file system" failed at line 2271 in ..\Middlewares\Third_Party\LwIP\src\apps\httpd\httpd.c " .
I find it is in file "httpd_opts.h", " LWIP_HTTPD_DYNAMIC_HEADERS" is not defined.
From Cube ==>Configuration ==>LWIP ==> HTTPD, nowhere can I define " LWIP_HTTPD_DYNAMIC_HEADERS".
Any suggestions?
Solved! Go to Solution.
2018-10-25 2:06 AM
Hi @Zhang.Sam
You can activate this define from the LWIP configuration window
Open the configuration window
Switch to HTTPD tab
Enable LWIP_HTTPD
Search for the needed parameter and you will found it (be sure the advanced checkbox is checked)
2018-09-18 11:33 PM
This refers to the method how the files which are to be served are stored - with or without the headers sent out before the "webpage" itself.
In the "normal" incarnations of lwip there's a utility attached to be used to generate the "filesystem", called makefsdata, that can generate the "filesystem" (fsdata.c) with or without the headers. In the generated fsdata.c, every "file" has a fsdata_file struct which describes that "file", and one of its fields is http_header_included (which, while declared as u8, is in fact a boolean value). The assert above says, that "header for this file is not included, and I don't know how to generate headers dynamically".
Quoting from httpd.c:
* By default, the server assumes that HTTP headers are already present in
* each file stored in the file system. By defining LWIP_HTTPD_DYNAMIC_HEADERS in
* lwipopts.h, this behavior can be changed such that the server inserts the
* headers automatically based on the extension of the file being served. If
* this mode is used, be careful to ensure that the file system image used
* does not already contain the header information.
*
* File system images without headers can be created using the makefsfile
* tool with the -h command line option.
I don't Cube/CubeMX so can't comment on what you can or cannot achieve by wildly clicking.
JW
2018-10-25 2:06 AM
Hi @Zhang.Sam
You can activate this define from the LWIP configuration window
Open the configuration window
Switch to HTTPD tab
Enable LWIP_HTTPD
Search for the needed parameter and you will found it (be sure the advanced checkbox is checked)