2025-01-20 02:03 PM
Hi developers.
I have the same issue as many others, which has been posted already 4-5 times and marked as "solved" in some of them, but it is not at all the case.
The CubeMX on launsching shows the first screen (splash) and then disappears.
It worked a couple of times after intallation, then again after de-installation/reboot/re-installation/reboot.
Watching the Task-Manager it shows a process called "OpenJDK Platform binary" which starts at high CPU and ends up to 0% but with around 200MB RAM reserved. And this can take place many times, collecting a bunch of idle/useless processes. I run it with Windows 10, latest version of JAVA and CUBE at this moment, but with a previous version on both I used to have the same issue.
While unistalling, I try to find every single file I can, so that I delete each trace manually, but every time I re-install it, it still "knows" which was my last opened projects and which uC I use.
Maybe ST can see it a bit seriously the topic. I suppose I am not the only one trying not to switch to another microcontroller, but if I cannot develop with ST, then I have to move on with my next projects differently.
Thanks for your precious time!
2025-01-20 02:36 PM
Yes, failing silently is unacceptable. It really needs to provide a breakdown of exactly what's wrong or missing. And probably providing a comprehensive diagnostic, repair and remove option or function.
2025-01-21 12:30 AM
2025-01-21 01:22 PM
Hello Souhaib, thanks for asking.
My current system:
-CubeMX 6.13.0
-Windows 10, Enterprise
-(java 8u431)
Previously I had on the same laptop
-CubeMX 5.1.0
-(java 8u211)
Just for the story:
I hadn't used Cube since over a year. I started again 1 month ago and this thing happens. I searched the issue online and thought maybe time for an upgrade (which I am not a fan to do so, obvious reasons) and brought it to the latest state. Problem occured again and reinstalled it, worked, stopped working, uninstalled, installed, worked two times and here I am.
Question (don't know if relevant):
how can I delete all traces of Cube when I uninstall? I tried to find evry single folder but every time I reinstall, Cube "knows" my preferences (a good spy). Does it have to do with the registry or with my profile on ST?
Debugging regards
2025-01-27 01:05 PM
Every day I try to start CubeMX 4-5 times and same story: splash screen shows up and disappears..
Except yesterday! I just unexpectally opened.
I don't know how relevant it is, but it did after closing the MozillaFirefox.
Today I tried to replicate this:
open Mozilla->close Mozilla->Cube first attempt failed -> Cube second attempt succeeded
Maybe a coincidence (?)
2025-01-27 04:45 PM
Java dislikes unsuitable locale settings. Try changing language and running it with a different locale