cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 CubeMX - Generate Code fails on a Mac

chairdeng
Associate II

Hi All

I have installed STM32 CubeMX on a Mac and I get the following error when trying to generate code:

The Eclipse executable launcher was unable to locate its companion shared library.截屏2024-12-01 18.42.46.png

22 REPLIES 22

Using CubeIDE for project generating was the only possible solution. I just updated my macOS to 15.2 (24C101) yesterday, but someone else mentioned 15.1.1 as well. A downgrade of CubeMX didn't worked for me. 

Souhaib MAZHOUD
ST Employee

Hello,

This behavior is under investigation by development team and tracked by the Ticket 198693 (for internal follow-up) and that will be fixed as soon as possible.
STM32CubeIDE can be used for project generation on macOS 15.1 and 15.2 as a temporary solution.

KR,

Souhaib

Hello, what is the latest progress?