2024-12-01 02:43 AM
Hi All
I have installed STM32 CubeMX on a Mac and I get the following error when trying to generate code:
The Eclipse executable launcher was unable to locate its companion shared library.
2024-12-13 03:45 AM
Using CubeIDE for project generating was the only possible solution. I just updated my macOS to 15.2 (24C101) yesterday, but someone else mentioned 15.1.1 as well. A downgrade of CubeMX didn't worked for me.
2024-12-13 05:32 AM
Hello,
This behavior is under investigation by development team and tracked by the Ticket 198693 (for internal follow-up) and that will be fixed as soon as possible.
STM32CubeIDE can be used for project generation on macOS 15.1 and 15.2 as a temporary solution.
KR,
Souhaib
2024-12-22 06:28 PM
Hello, what is the latest progress?
2024-12-29 12:33 AM
Unfortunately, as written here before, going back to version 6.12.1 does not fix the situation. The work has stopped. Please give this problem priority time.
2025-01-02 11:08 PM
Use Volume-Shared Virtual Machine applications (e.g. Parallels Desktop or something else) to run CubeMX on Windows to generate initial code might be a temporary workaround for this issue.
2025-01-03 05:41 AM
Hello
We apologize for the issues created by the misbehavior of STM32CubeMX.
We are currently analyzing the root cause and we are given it high priority in order to provide a solution ASAP.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.