2021-03-31 03:30 AM
In CubeMX the name for the Automatic Retransmission of CAN-Messages is named:
"NO-AUTOMATIC Retransmission"and is set to "DISABLE"
When reading this I interpreted it as: Automatic Retransmission is done if set to DISABLE
In the generated code however the corresponding setting is:
hcan1.Init.AutoRetransmission = DISABLE;
Which leads to "no Automatic retransmission" and therefore to missing messages in case of high busload !!!
Please correct the wording in STMCubeMX so other users are not falling into the same problem.
BR GS
Solved! Go to Solution.
2021-03-31 04:25 AM
Hi @GS@S ,
I advise you to update and use the latest release of STM32CubeMX v6.2.0 which contains the correct wording
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
Imen
2021-03-31 03:49 AM
Hello @GS@S ,
Which CubeMx and Cube HAL release are you using ?
Imen
2021-03-31 04:25 AM
Hi @GS@S ,
I advise you to update and use the latest release of STM32CubeMX v6.2.0 which contains the correct wording
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
Imen
2021-03-31 05:42 AM
I am already using Version 6.2.0!
However the project was created with FW_F4 V1.24.1. The missing CAN messages were detected now after the project is released to customers already.
Ok, and after updating the HAL release FW_F4 V1.24.1 to V. 1.26.0 the wording now is correct.
I am always careful when changing to new releases of HAL, because I encounter too often that problems arise with new releases which I often can't see in the fist place...
Did not think the HAL release would change the behaviour of Cube Setup menu entries...
Thank you for the support.
2021-03-31 06:28 AM
... Ok, and now exactly the mentioned and feared scenario happened:
After updating my project to the latest release the USB Virtual COM port communication is no longer working ... USB is detected, but communication no longer possible. :/
Will switch back to the previous HAL release setup!