Simulink error for programming ST Nucleo board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-04 2:28 AM
Hi,
I want to program my STM32H753ZI Nucleo board with Simulink. I successfully programmed it to blink an LED. However, I get the following error when I try to enable a timer (for PWM, or Encoder).
C:/ProgramData/MATLAB/SupportPackages/R2023b/toolbox/shared/supportpackages/stm32/src/rtiostream_serial.c:10:10: fatal error: rtiostream.h: No such file or directory
10 | #include "rtiostream.h"
| ^~~~~~~~~~~~~~
compilation terminated.
gmake: *** [rtiostream_serial.o] Error 1
I have tried this with both CubeMx 6.4 and 6.10 (Matlab has recommended to use CubeMx 6.4.).
I have also tried the STM32F446RE Nucleo board and the same error emerged.
Any suggestions to solve this problem are highly appreciated.
Thanks
- Labels:
-
STM32F4 Series
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-19 3:01 AM
Similar problem I am having, Windows 11 23H2, Matlab R2023b. I am using a STM32G431KB board.
...\Desktop\xxx\Software_Projects\sakin_ert_rtw>if "all" == "" ("C:\PROGRA~1\MATLAB\R2023b\bin\win64\gmake" -f sakin.mk all ) else ("C:\PROGRA~1\MATLAB\R2023b\bin\win64\gmake" -f sakin.mk all )
"C:/ProgramData/MATLAB/SupportPackages/R2023b/3P.instrset/gnuarm-armcortex.instrset/win/bin/arm-none-eabi-gcc" -ffunction-sections -fdata-sections -Wall -MMD -MP -MF"stm_adc_ll.dep" -MT"stm_adc_ll.o" -c -O0 -mcpu=cortex-m4 -mthumb -mlittle-endian -mthumb-interwork -mfpu=fpv4-sp-d16 -mfloat-abi=hard -DMW_ADC1_ENABLED=1 -DMW_ADC1_VAR=mw_adc1 -DMW_TIM1_ENABLED=1 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DUSE_FULL_LL_DRIVER -DSTM32G431xx -DUSE_HAL_DRIVER -DMW_TIMEBASESOURCE=TIM2 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DTID01EQ=0 -DXCP_CUSTOM_PLATFORM -D__FPU_PRESENT=1U -D__FPU_USED=1U -DMW_FREERTOS -DMW_EXTMODE_STACKSIZE=1024 -DSTACK_SIZE=64 -DRT -DOS_STKSIZE=128 -DMODEL=sakin -DNUMST=2 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 @sakin_comp.rsp -o "stm_adc_ll.o" "C:/ProgramData/MATLAB/SupportPackages/R2023b/toolbox/shared/supportpackages/stm32/src/stm_adc_ll.c"
In file included from C:/Users/xxx/Desktop/xxxxx/Software_Projects/sakin_ert_rtw/MW_target_hardware_resources.h:7,
from C:/ProgramData/MATLAB/SupportPackages/R2023b/toolbox/shared/supportpackages/stm32/src/stm_adc_ll.c:5:
C:/Users/xxxx/Desktop/xxxxx/Software_Projects/sifirdan/Core/Inc/main.h:30:10: fatal error: stm32g4xx_hal.h: No such file or directory
30 | #include "stm32g4xx_hal.h"
| ^~~~~~~~~~~~~~~~~
compilation terminated.
gmake: *** [stm_adc_ll.o] Error 1
Simulink generates a tlc file but as soon as GNU Tools for ARM Embedded Processors toolchain starts to build the code, it just cannot read any headers starting with the HAL driver headers. Even though they are right next to the .ioc file at the same folder, same path, without spaces in the path.
Honestly this is driving me crazy. I have contacted local Matlab support and waiting for a response.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-19 6:35 AM
Hi,
Yes, it is a weird problem. Indeed, I tried it on another computer and it compiled successfully. The CubeMX seems to be the source of this problem. I can suggest two approaches:
1. Adding the header files manually.
2. Installing the latest version of CubeMx.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-19 11:45 AM - edited ‎2024-03-17 12:32 PM
Hi,
Matlab does not recommend using a newer version of the CubeMX than the 6.4 version. That's why I am not updating it.
I honestly don't think it is CubeMX's fault. I use the same version CubeMX on my other computer (had to start using my old laptop for this) and everything works well. CubeMX outputs are the same in both computers.
I am suspecting GNU Embedded compiler version is not compatible with something but I don't know what.
SOLVED
edit: The root of the problem was other cubemx project folders were present in Matlab's path. Do not add .ioc folders to path of the compiler.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-24 5:18 PM
No chance to install the new CubeMX, SIMULINK is asking for v6.4.0; otherwhise it cannot validate the SW and sh*t will hit the fan~
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-24 5:52 PM
Yes, this is the right solution, thank you!!