2023-04-18 5:31 AM
Hi... for some reasons I cant regenerate my code from CubeMx but I need to change crystal 8M to oscillator 14.7456... in spite of replacing the clock function (void SystemClock_Config(void) ) with new one, my project does not work. what other changes do I need to consider for changing the clock in a project generated by CubeMx?
thank you in advance
Solved! Go to Solution.
2023-04-19 8:29 AM
Hello @Zakba.1
If your project contains any code that is sensitive to timing (e.g delay loops...), you may need to update this code and consider the new oscillator frequency.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-18 7:25 AM
Well, why not generating 2 new dummy projects with the old and new settings and comparing the output. The new freq. may be to high for the old (PLL?) settings, and oscillator != crystal ?
hth
KnarfB
2023-04-18 4:44 PM
Well I tried that creating a dummy project with new clock configuration and replaced the generated system clock function with new one... this function as far as I know configures freq, pll, crystal or oscillator type in itself... except this function do I need to change any other configs in project?
Ps: I generated the code in cube with HAL lib
Post edited to adhere community guidelines.
2023-04-19 8:29 AM
Hello @Zakba.1
If your project contains any code that is sensitive to timing (e.g delay loops...), you may need to update this code and consider the new oscillator frequency.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.