cancel
Showing results for 
Search instead for 
Did you mean: 

SDMMC with SD card and NUCLEO-L476 not working

PSmol.1
Associate II

Hi everyone,

I am having a hard time getting the SDMMC interface working with my NUCLEO-L476RG.

I feel like this should be an out-of-the-box solution using CubeMX, but somehow I can't get it to work.

I am getting a chip detect but an error when establishing the card voltage.

As for code, I am just using what CubeMX is giving me, SDMMC 1 bit wide (I tried 4bit, same situation), FATFS with SD card settings. For clock, the sdmmc clock is set to 36MHz (default) and clock divider of 16.

Any help is greatly appreciated!

0 REPLIES 0