Skip to main content
September 28, 2021
Question

SDcard remount fails when f_mount returns FR_NOT_READY

  • September 28, 2021
  • 0 replies
  • 818 views

Hello!

Using CubeMX6.2 I am functioning on Hal Library and STM32F427VI.I apply DMA and place SDMMC controller‘s clock frequency to 24MHz. In case of facing SD error during programming. By following below steps I get back on SD card:

1 - MX_FATFS_Init;

2 - HAL_SD_InitCard;

3 - result = f_mount(&FATFS, " ", 1);

These functions work successfully and normally outcome turns to FR_OK but some time result turns to FR_DISK_ERROR. Before mounting SD card if we face issues the consequences returns FR_DISK_ERROR or FR_NOT_READY and will never sort out by following above functions.

If before mounting Sd card I unplug it and after that mount and find FR_not_ready then connect SD and remount it. This issue also occurs in case of switching MicroSD pins in ESP8266 and STM32. At last I unplug – connect MicroSD or to solve the issue by the function of reset micro.

To complete my project it’s very important to remount SD card. I hope any one will help me.

Thanks

This topic has been closed for replies.