cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with CubeMX

Not applicable

Hello!

I am working on STM32 (H7) project , when I click OC file it creates STM32CubeMX and it develop a dialogue which ask, with the help of STM32Cube firmware FW_H7 V1.9.0 this project was designed. With the usage of STM32Cube firmware version FW_H7 V1.9.0. the function of new STM32Cube V6.3.0 is better.

I have a confusion I am at V1.9.0, already , but in case if I choose <Migrate> then make Cube MX return back with <Generate Code>.With the redesigning of project the floating point variables ‘ output no more working.

Instead of Migrate if I choose continue Cube MX shows an empty screen

STM32CubeIDE is v1.7.0

I want suggestions regarding this problem.

Thank You.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Mouadh JERIDI
Associate III

Hello @Enora.1​  !

Can you please provide me with your IOC file ?

Thank you,

Mouadh.