2017-01-12 1:59 AM
Hi !
First, I use the version 4.18.0 STM32Cube V1.0, and Atollic True Studio 7.0.1, so both are (normally) the last ones.
I try to generate, with CubeMX, a project on STM32F417VG, using several libraries, the STM32_USB_HOST_LIBRARY for MSC being one of them. My problem is that I cannot use this project !
I generate the project -> I compile -> Works !
I generate the project -> I add these lines in the main.h :
&sharpinclude ''usbh_def.h''
USBH_HandleTypeDef hUSBHost;
I doesn't change anything else, and I don't write anything else but it doesn't compile, I have some strange errors.
Four of them are about four different macros (USBH_MAX_DATA_BUFFER, USBH_MAX_NUM_ENDPOINTS, USBH_MAX_NUM_INTERFACES, USBH_MAX_NUM_SUPPORTED_CLASS) in the file ''usbh_def.h'' with this message :
Macro undeclared here (not in a function)
But those macros are declared in usbh_conf.h which is directly included in usbh_def.h.
Another error is :
USBH_DeviceTypeDef has no member name 'CfgDesc_Raw'
in this line :
And when I go to the definition of USBH_DeviceTypeDef, I have this :
So if we want CfgDesc_Raw, it's because USBH_KEEP_CFG_DESCRIPTOR == 1 (and I checked, it's true), but if we don't have it in the structure, it's because the same macro != 1...
What happened ? Why can't I use this library properly ? Do you have any solution I can try, please ?
Thanks !
Regards,
Antoine
#cubemxSolved! Go to Solution.
2017-01-12 9:36 AM
Hello Antoine,
I could reproduce a compilation issue with Attollic, IAR and Keil but looks a bit different.
What is failing is the compilation of usbh_conf.c after adding the 2 lines in main.h
This seems to be linked to a recent change in code generation:
In generated stm32f4xx_hal_conf.h there is the line
#include 'main.h'
In older version of Cube there was instead
#include 'mxconstants.h'
If I remove this include main.h, compilation of usbh_conf.c is ok.
The error I get is:
In file included from ../Inc/main.h:49:0,
from ../Inc/stm32f4xx_hal_conf.h:43, from ../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal.h:48, from ../Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f4xx.h:245, from ../Inc/usbh_conf.h:55, from ../Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_core.h:37, from ../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc/usbh_msc.h:37, from ..\Middlewares\ST\STM32_USB_Host_Library\Class\MSC\Src\usbh_msc.c:42:../Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:281:44: error: 'USBH_MAX_NUM_ENDPOINTS' undeclared here (not in a function) USBH_EpDescTypeDef Ep_Desc[USBH_MAX_NUM_ENDPOINTS];Actually usbh_conf.h which defines the
USBH_MAX_NUM_ENDPOINTS is itself including stm32f4xx.h which leads to include main.h. So in main.h you include a header file
As a workaround I would suggest adding your lines in the main.c file if possible or create another header file if you need to share this with another source file.
Jocelyn
2017-01-12 8:21 AM
Hi
WAJNTRAUB.Antoine
,I tried the same using Keil and didn't got any compilation issue.
In order to be in the same configuration conditions, please share your IOC file. I'll give it a try using TrueStudio.
Then as general recommendation to generate Host example, please refer to UM1718:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-01-12 9:36 AM
Hello Antoine,
I could reproduce a compilation issue with Attollic, IAR and Keil but looks a bit different.
What is failing is the compilation of usbh_conf.c after adding the 2 lines in main.h
This seems to be linked to a recent change in code generation:
In generated stm32f4xx_hal_conf.h there is the line
#include 'main.h'
In older version of Cube there was instead
#include 'mxconstants.h'
If I remove this include main.h, compilation of usbh_conf.c is ok.
The error I get is:
In file included from ../Inc/main.h:49:0,
from ../Inc/stm32f4xx_hal_conf.h:43, from ../Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal.h:48, from ../Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f4xx.h:245, from ../Inc/usbh_conf.h:55, from ../Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_core.h:37, from ../Middlewares/ST/STM32_USB_Host_Library/Class/MSC/Inc/usbh_msc.h:37, from ..\Middlewares\ST\STM32_USB_Host_Library\Class\MSC\Src\usbh_msc.c:42:../Middlewares/ST/STM32_USB_Host_Library/Core/Inc/usbh_def.h:281:44: error: 'USBH_MAX_NUM_ENDPOINTS' undeclared here (not in a function) USBH_EpDescTypeDef Ep_Desc[USBH_MAX_NUM_ENDPOINTS];Actually usbh_conf.h which defines the
USBH_MAX_NUM_ENDPOINTS is itself including stm32f4xx.h which leads to include main.h. So in main.h you include a header file
As a workaround I would suggest adding your lines in the main.c file if possible or create another header file if you need to share this with another source file.
Jocelyn