Problem with CubeMX after upgrading - can't open ioc file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 06:48 AM - edited ‎2023-12-07 07:36 AM
I upgraded STM32CubeIDE to 1.14.0 and then when I went to open an ioc file I got this message:
This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1.
There are two options to proceed:
-Migrate:Migrate your project using the current STM32CubeMX version (6.10.0)
-Continue: Continue to stay compatible with the old STM32CubeMX version 6.9.2
I chose the 'Migrate' option, which was probably a mistake. Now when I try to open the ioc file it just goes blank. Any advice please?
ADDED LATER: In the meantime, I tried opening a different project, but selected the 'Continue' option. Again I got a blank tab when I tried to open the .ioc file
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-08 02:15 AM
OK, I seem to have solved the problem by using X11 instead of Wayland.
I remembered that to get the previous version to work I had to change the .desktop file to use X11 instead of Wayland. I have now done the same thing for version 1.14.0 and the MX configuration program now works.
I can't say I understand it - but it's working.
Thank you responders!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 07:06 AM
Hello @Dabbo
Can you add your .ioc file so I can test it. I've tested with a personal project and it works fine for me.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 07:24 AM
Hi STTwo-32, and thanks for replying so quickly. The file is attached
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 07:28 AM
I got a warning that the file contents did not match the file extension, so I'm going to try again but changing extension from .ioc to .txt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 07:35 AM
can you share your .ioc file and not the .txt file.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 07:41 AM
This is the .ioc file with the file extension changed because the forum software would not accept it with the .ioc extension. I got a big red warning. Please just change the extension back from .txt to .ioc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-07 08:14 AM
Hello again
this works as supposed to be for me.
can you restart your PC and retry. It may solve your issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-08 12:25 AM
What is the current version of your installed STM32G0 FW ?
Have you tried to force the tool version by hand in the ioc file ? I know this is not always recommended and could be risky, but this could be worth trying...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-08 01:03 AM
Restarting PC - same problem.
Purged the STM32CubeIDE package from system and re-installed - same problem.
I'm puzzled by the message that said "This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1" as this device is F411CEU6 not the G0 series. Is that a clue to the problem?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-12-08 01:05 AM
Hi Oscar. Thanks for replying.
Which line in the ioc file would need editing?
I'm puzzled by the message that said "This project was setup with STM32CubeMX V6.9.2 using STMCube FW_G0 V1.6.1" as this device is F411CEU6 not the G0 series. Is that a clue to the problem?