cancel
Showing results for 
Search instead for 
Did you mean: 

No GPIO on Nucleo-G071RB Pinout and Configuration

NR-A Comm
Associate II

STM32CubeMX Board Selector does NOT show NUCLEO-G071RB, so I select MCU Selector and search STM32G071RB. STM32CubeMX shows NUCLEO-G071RB on Board Colum.

I click NUCLEO-G071RB and I Start Project, Initializing all peripherals with their default Mode YES.

Pinout & Configuration is shown but there is NO GPIO such as LD4 (PA5), SW4 (PC13).

Question: Is this NO GPIO correct or BUG?

My Environment is, STM32CubeMX: 5.1.0, STM32G0 package: 1.1.0, TrueSTUDIO: 9.3.0.

4 REPLIES 4
Dvorak.Peter
Senior II
NR-A Comm
Associate II

Thank you very much for your response.

I understood that GPIO additional setting of LD4(PA5) and GPIO_EXTI13 mode setting change of B1(PC13).

By the way, each Lab is using MDK-ARM. In addition, I am worried that there is no TrueSTUDIO in the sample project outline of P57.

Is not recommended to develop STM32G0 with TrueSTUDIO?

Hi @NR-A Comm​ 

Thank you @Dvorak.Peter​  for you quick reply.

@NR-A Comm​ Until now STM32G0 does not support TrueSTUDIO, this will be available in the next version.

Best regards,

Nesrine.

Thank you for your answers, Nesrine and Dvorak.

I understood STM32CubeMX and TrueSTUDIO well.

Best ​ regards, NR-A Comm.