cancel
Showing results for 
Search instead for 
Did you mean: 

Mounting USB using fatfs

alex_embedded
Associate III

Hi all,

I am having troubles mounting a USB using the "f_mount" function in the fatfs library.

My usb does mount but only after many attempts, using a simple counter I have found it to be 81, every single time I run the code it is the same amount of attempts.

Once mounted it works flawlessly and as I expect, however I am struggling to understand why it is taking so many attempts to mount.

I have a "dirty" function to test writing to a file, shown below:

void USB_WriteTest(void){
 
		  // Attempt to mount usb
		  if(f_mount(&USBHFatFS, USBHPath, 1)==FR_OK){
 
			  HAL_Delay(100);
			  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Mount Success...\r\n", strlen("Mount Success...\r\n"));
 
			  //Name of file being created
			  char myFileName [] = "config.txt";
 
			  // Open a file to write to
			  if(f_openAppend(&USBHFile, myFileName)==FR_OK){
 
				  HAL_Delay(100);
				  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Open Success...\r\n", strlen("Open Success...\r\n"));
 
				  // Message to save to usb
				  char logMsg[] = "Hello world!!\r\n"
						  	  	  "Sent from nucleo to USB\r\n";
 
				  // Length of message
				  int logLength = strlen(logMsg);
 
				  // Write data to the usb
				  if(f_write(&USBHFile, logMsg, logLength, &USBBytes)==FR_OK){
 
					  HAL_Delay(100);
					  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Write Success...\r\n", strlen("Write Success...\r\n"));
 
				  }
				  else{
 
					  HAL_Delay(100);
					  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Write Failed!\r\n", strlen("Write Failed!\r\n"));
				  }
 
				  //close the file after use
				  f_close(&USBHFile);
 
			  } // end f_open
			  else{
 
				  HAL_Delay(100);
				  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Open Failed!\r\n", strlen("Open Failed!\r\n"));
			  }
 
			  HAL_Delay(100);
			  f_mount(0,"", 0);
 
		  } // end f_mount
		  else{
 
			  HAL_Delay(100);
			  HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Mount Failed!\r\n", strlen("Mount Failed!\r\n"));
		  }

I have called it in my main loop in an if statement so it will only run when a USB is connected, example below:

// Check if a USB is connected
 if(hUsbHostFS.device.is_connected==1){ 
      // USB write test function. Writes a string to a txt file
      USB_WriteTest();
 }

Any help would be greatly appreciated!

4 REPLIES 4

Consider doing this as a subroutine, lot of repetitive code

HAL_Delay(100);

HAL_UART_Transmit_IT(&huart3, (uint8_t*)"Mount Success...\r\n", strlen("Mount Success...\r\n"));

The top level interactions aren't going to be very instructive. Instrument the DISKIO layer, and look at what is happening there, especially the errors and the data returned from MBR and BPB.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Pavel A.
Evangelist III

I've noticed a similar issue too, with STM32F4 (custom board).

After poll for if(hUsbHostFS.device.is_connected==1) succeeds, there are few "glitches" and is_connected changes state, until it stabilizes. On my device the number of these "glitches" is much less, about 2-3,

So I just retry several times until mount and file operations succeed.

If someone could explain this, would be great.

-- pa

alex_embedded
Associate III

@Pavel A.​ 

Sorry to bring this up again but did you further your understanding as to why this is happening?

I still haven't :(

Pavel A.
Evangelist III

> Sorry to bring this up again but did you further your understanding as to why this is happening?

No I have not returned to this project since then. Other threads advice to update the fatfs library from upstream.

-- pa