cancel
Showing results for 
Search instead for 
Did you mean: 

Missing Pin PD2 on STM32L433RCTxP

SWend
Associate II

Hey,

I´m confused why i can not use Pin PD2 on Cube MX on the Nucleo Board L433RC even though it should actually exist because it exist when you select another STM32L433.

Without that Pin, i can´t use SDMMC. If i select for example the STM32L433RCTx, there is the Pin PD2. But if i try to use it with the Nucleo it wont work.

Any suggestions?

10 REPLIES 10
Khouloud ZEMMELI
ST Employee

​Hello @SWend​ 

This is reported internally for further check.

Best Regards,

Khouloud