cancel
Showing results for 
Search instead for 
Did you mean: 

Missing Pin PD2 on STM32L433RCTxP

SWend
Associate II

Hey,

I´m confused why i can not use Pin PD2 on Cube MX on the Nucleo Board L433RC even though it should actually exist because it exist when you select another STM32L433.

Without that Pin, i can´t use SDMMC. If i select for example the STM32L433RCTx, there is the Pin PD2. But if i try to use it with the Nucleo it wont work.

Any suggestions?

1 ACCEPTED SOLUTION

Accepted Solutions

There is not exist PD2 for STM32L433RCTxP but for STM32L433RCTx mcu

is also obvious from schematic you published. PD2 leads to an open solder bridge.

Also there is no SDMMC interface in STM32L433RCTxP mcu.

P makes the difference

View solution in original post

10 REPLIES 10
S.Ma
Principal

Do you confirm PD2 exist on the Nucleo schematic?

SWend
Associate II

yes

SWend
Associate II

0690X000008A5L5QAK.png

SWend
Associate II

0690X000008A5MhQAK.png

That looks a little bit Strange. What DNF means? Do not fit?

There is not exist PD2 for STM32L433RCTxP but for STM32L433RCTx mcu

is also obvious from schematic you published. PD2 leads to an open solder bridge.

Also there is no SDMMC interface in STM32L433RCTxP mcu.

P makes the difference

SWend
Associate II

ok, thanks. So i cant test SDMMC with L433RC without making my own board?

Perhaps try a NUCLEO-L476RG, and replace the chip.

Try asking your FAE to create one.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal

Find on the datasheet the pins which have SDMMC signals and which package gots it.

Maybe Discovery board if there is has microSD socket and signals wired.

SWend
Associate II

ok, do you know the meaning of the two configs on the right side of the schematic?

Can i use PD2 when i solder the bridge?