2020-01-17 1:31 AM
Dear customers,
We are facing a little issue during the migration from the 5.4.0 to the 5.5.0 (reported in this thread https://community.st.com/s/question/0D50X0000BxzZV9SQM/upgraded-stm32cubemx-from-540-to-550-and-now-it-fails-to-generate-the-project)
To avoid having this problem, please migrate to the 5.5.0 by installing the new package from the web and not updating from the tool.
Best regards,
STM32CubeMX team
2020-01-20 5:15 PM
I'm using 5.5.0 and want to import a 5.4.0 project but the Import Project is grayed out. This is a fresh install
2020-01-22 12:19 AM
Hello @Community member
Import do work only on a fresh loaded MCU, importing on a configured MCU (like in the screenshot) will be available in a future release of MX
2020-02-12 4:14 AM
I firstly removed the 5.5.0 which was installed via update tools and then install 5.5.0. However, it still failed to generate the project.
2020-02-24 12:21 PM
I have the same problem
2020-02-24 11:25 PM
I guess you are using Java13. If yes, please remove this version and install at least Java11 or Java8. We found an issue with Java13/Keil IDE, this issue is not related to STM32CubeMX upgrade process.
For info: STM32CubeMX is not yet validated/tested with Java13.
2020-03-04 5:22 AM
The new 5.6.0 with Java 8 still has the same error.