cancel
Showing results for 
Search instead for 
Did you mean: 

Migration issue from 5.4.0 to 5.5.0

Nawres GHARBI
ST Employee

Dear customers,

We are facing a little issue during the migration from the 5.4.0 to the 5.5.0 (reported in this thread https://community.st.com/s/question/0D50X0000BxzZV9SQM/upgraded-stm32cubemx-from-540-to-550-and-now-it-fails-to-generate-the-project)

To avoid having this problem, please migrate to the 5.5.0 by installing the new package from the web and not updating from the tool.

Best regards,

STM32CubeMX team

6 REPLIES 6
Karl Yamashita
Lead III

I'm using 5.5.0 and want to import a 5.4.0 project but the Import Project is grayed out. This is a fresh install

0690X00000BwFjLQAV.jpg

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
Nawres GHARBI
ST Employee

Hello @Community member​ 

Import do work only on a fresh loaded MCU, importing on a configured MCU (like in the screenshot) will be available in a future release of MX

Zoey
Associate III

I firstly removed the 5.5.0 which was installed via update tools and then install 5.5.0. However, it still failed to generate the project.0690X00000D9kegQAB.png

1kvin
Associate

I have the same problem0690X00000DXDEEQA5.jpg

I guess you are using Java13. If yes, please remove this version and install at least Java11 or Java8. We found an issue with Java13/Keil IDE, this issue is not related to STM32CubeMX upgrade process.

For info: STM32CubeMX is not yet validated/tested with Java13.

The new 5.6.0 with Java 8 still has the same error.​