cancel
Showing results for 
Search instead for 
Did you mean: 

LTDC: Non-editable Total Width and Total Height are short of 1 pixel?

Ricko
Senior III

Hi,

looking at the screenshot below of CubeMX in the LTDC, the total Width and total Height are non-editable (i.e. auto calculated) but they are one pixel less?

For example, for the attached display datasheet:

- Horizontal Sync Width (Editable) = 8 pixels

- Horizontal Back Porch (Editable) = 7 pixels

- Active width (Editable) = 800 pixels

- Horizontal Front Porch (Editable) = 6 pixels

So the total is 821 pixels instead of 820. But CubeMX displays 820 and it is not editable.

Did I miss something? Do I need to change some other setting?

Thank you :)

 

Ricko_0-1741474238541.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Ricko
Senior III

The window at the bottom was hidden so I assumed there was no "tooltip" explanation. NowI see it at the bottom, it does say how it is calculated

 

Ricko_0-1741474804709.png

 

View solution in original post

1 REPLY 1
Ricko
Senior III

The window at the bottom was hidden so I assumed there was no "tooltip" explanation. NowI see it at the bottom, it does say how it is calculated

 

Ricko_0-1741474804709.png