2016-11-22 10:17 PM
Hello all, has anyone successfully installed CubeMX 4.17.0 on Mac OSX Sierra (10.12.1)? Every time I doubleclick the install it just bounces and then nothing happens. Any suggestions?
#cubemx-macos-sierraSolved! Go to Solution.
2018-05-06 11:51 PM
Solution Found For Those With macOS High Sierra
First open this macro file inside the zipped package `
en.stm32cubemx
`. `./en.stm32cubemx/SetupSTM32CubeMX-4.25.0.app/Contents/MacOs/
SetupSTM32CubeMX-4_25_0_macos
`, this will open the installer.
It will by default try to install to `
/usr/share/applications.
`. This is incorrect. You need to find your application directory.```
MacBook-Pro:en.stm32cubemx briankhuu$ cd ~/Applications/
MacBook-Pro:Applications briankhuu$ pwd
/Users/briankhuu/Applications
```
In my case it was `
/Users/briankhuu/Applications
`, you can then modify the application install directory during the install prompts.This will then successfully install CUBEmx in macOS High Sierra.
Hope it helps
2016-11-23 1:04 AM
Hello,
Refer to the user manual for STM32CubeMX and follow the steps/requirements for MacOS: Make sure you have administrators rights.- Software requirements For MacOS, install Java Development Kit 1.7.0_45 or later.Regards2016-11-23 12:48 PM
Yes, you need to install Java.
On Sierra it works great, less filling (actually just the same)2016-11-24 11:05 PM
I have both Java Developer packages and admin rights on my machine but still no joy. What did end up working for me though was to right-click on the .app installer and open up the package contents. Inside the MACOS folder there is a Setup... binary file, double-clicked it and magically the terminal pops up with a install script and voila it installs, weird.
Hope this helps someone else.2016-12-05 6:21 PM
I also had this problem on Sierra. Installed JDK, restarted, and the installer would quit without opening the wizard.
Ferguson.Samuel
has the result that worked for me. The second time I opened the binary in the terminal, the wizard opened, and I was able to install.2017-05-11 6:23 PM
Thank you. This worked.
I am on macOS Sierra2017-05-19 2:59 AM
I also saw that it worked only the 2nd time I launched it.
It did complain that it could not find /usr/share/applications.
Indeed that is a path which does not exist, and which the finder will not let me create.
2018-05-06 11:51 PM
Solution Found For Those With macOS High Sierra
First open this macro file inside the zipped package `
en.stm32cubemx
`. `./en.stm32cubemx/SetupSTM32CubeMX-4.25.0.app/Contents/MacOs/
SetupSTM32CubeMX-4_25_0_macos
`, this will open the installer.
It will by default try to install to `
/usr/share/applications.
`. This is incorrect. You need to find your application directory.```
MacBook-Pro:en.stm32cubemx briankhuu$ cd ~/Applications/
MacBook-Pro:Applications briankhuu$ pwd
/Users/briankhuu/Applications
```
In my case it was `
/Users/briankhuu/Applications
`, you can then modify the application install directory during the install prompts.This will then successfully install CUBEmx in macOS High Sierra.
Hope it helps
2018-07-02 7:06 AM
You are the best, thanks !