cancel
Showing results for 
Search instead for 
Did you mean: 

Issue to select TouchfGx 4.24.1 version in CubeMx

Kenwang
Associate III

I use touchfgx 4.24.1 Designer to generate a new project. After generating it, I use this stm32cubemx 6.12.1 to open the stm32cubeProject. It will say that my stm32cubemx 6.12.1 does not have touchfgx 4.24.0 installed, and it wants me to install touchfgx 4.24. 0.
My question is, I obviously used the 4.24.1 version of the project, why do I need to install touchfgx 4.24.0 when opening the stm32cubeProject project in stm32cubemx 6.12.1? I am sure that my stm32cubemx has touchfgx 4.24.1 installed.

Kenwang_0-1728385608778.png

 

Kenwang_1-1728385664740.png

 

 

11 REPLIES 11
SofLit
ST Employee

Hello,

Don't know if you have used the version 4.24.0 before, but try to set the TouchGFX version from "Select components":

SofLit_2-1728484644573.png

Then:

 

SofLit_0-1728484581244.png

Finally, accept the migration:

SofLit_3-1728484705388.png

At this stage TouchGFX V4.24.1 is set to your project.

Hope it helps.

 

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

I previously used version 4.24.0, but I have since removed it from my computer. Currently, I only have version 4.24.1 installed.

After installing version 4.24.1, I created a new project. However, when I opened the project in STM32CubeMX to configure the RTC and ADC settings, it indicated that the TouchGFX version in use is 4.24.0, not 4.24.1.

I find this quite puzzling since I clearly created the project using version 4.24.1. Why does STM32CubeMX report that the project was generated with version 4.24.0 and prompt me to install that version of TouchGFX?

Could it be that there was an issue with the parameters when TouchGFX generated the new project, leading to this discrepancy?

If you have created the project with TouchGFX V4.24.0, CubeMx will ask you to use that version unless you change the version to V4.24.1 like I show you in my previous comment.

Did you apply these steps?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Kenwang
Associate III

Maybe I didn't make it clear. I use version 4.24.1 to create a new project, so I expect that when I use cubemx to open it, cubemx will also know that I use version 4.24.1 to create the project. , instead of asking me to install version 4.24.0 of touchgfx.

You can do it manually as I described previously.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hello,

Did you solve the issue with the steps I described previously?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hi SofLit,

I recorded a video of the steps I took to create the project. In the video, you will find that I used 4.24.1 to create the project, but cbuemx thought I used 4.24.0 to create the project.

Hello @Kenwang ,

At the minute 1:54, you clicked on "Continue" button and you didn't select "Migrate", try to migrate.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

This is exactly where my problem lies. I clearly generated the project using version 4.24.1, but when I open it with CubeMX 6.12.1, it thinks the project was created with version 4.24.0. So, I believe there might be some settings in the code generator that weren't configured correctly, which is causing this issue?