2020-01-28 8:03 PM
I were trying to get data continues from a sensor and didnt find any flag that will acknowledge when a data is received . Only thing is there is HAL_UART_Receive_IT(),HAL_UART_Receive() functions.i need to seperate my data from Uart interupt handler.
2020-01-29 2:31 AM
how to enable USART1_IRQn interrupt....?
2020-01-29 5:30 AM
It is easy to write your own ISRs that conpletely skip all the hal callback faff.
Here's what i do:
1. Look in the interrupt vector table to get the name of the interrupt you want to use
2: declare a void [isr name] ( void ) function in your code. This is your isr.
3. Build the code and then delete/ comment out the old definition of the isr when the linker complains & rebuild.
This, of course, isn't the only approach, just what i did at first