cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to make friends HAL_TIM_PWM_Start_DMA (& htim1, TIM_CHANNEL_3, (uint32_t *) Buff, counter); with Repetition Counter.

Cheerful_Wind
Associate III

I tried on STM32F103C8Tx. The timer simply swallows the "repetition counter" of the DMA values ​​on the next update.

I was asked to make a simple example of playing a short wav file at a bit rate of 88 Kbps to attract the operator's attention.

The above design allows this to be done gracefully, but I would like to output the carrier frequency to ultrasound.

0 REPLIES 0