2023-09-07 10:55 AM - edited 2023-09-07 11:00 AM
Does anyone know how to import an IOC file into an existing project?
I was trying to have two IOC files; one for issue 1 of the hardware and one for issue 3 and swapping between them, but something's gone funky with it and now the project won't recognise the IOC file even though it's there in the directory.
If I move the two IOCs out of the project directory and then try and import them, but right clicking on the project, selecting import and then import IOC file, Cube spits its dummy out and tells me
"Project is already existing within current workspace" Whatever than means.
I have valid IOC files, why won't Cube accept them and what do I do to fix this please?
Ta.,
Solved! Go to Solution.
2023-09-07 11:07 AM
Looks like I've stumbled across it. Seems like File | Refresh is need.
Obv.
2023-09-07 11:07 AM
Looks like I've stumbled across it. Seems like File | Refresh is need.
Obv.