cancel
Showing results for 
Search instead for 
Did you mean: 

Incompatibility between X-CUBE-TOUCHGFX and X-CUBE-GNSS

PascalP
Associate II

Hello dear community,

I'm using a STM32U5A9J-DK.

I want to start in CubeMX a project based on this board, X-CUBE-TOUCHGFX and X-CUBE-GNSS softwares.

However, CubeMX warns me (in the "Software Packs Component Selector") that theses are incompatibles between them.

For example, if I choose X-CUBE-GNSS first then try to choose TouchGFX, it tells "This component cannot be selected: this application cannot be selected while the application from pack STMicrolectronics.X-CUBE-GNSS1.6.0.0 is selected":

PascalP_0-1725018811809.png

and vice versa.

I guess that is because the touch screen use PI6 (DSI_BL_CTRL) pin that can be used as reset pin or wake up pin for GNSS: is this correct ?

Is there a way to "force" or bypass this recommendation ?

Thanks a lot in advance for your help

 

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @PascalP 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

KR,

Souhaib