Question
Showing clock incompatibility while selecting USB_OTG_FS in STM32F205VE
Hai ,
I enabled USB_OTG_HS in STM32F205VE and default frequency as 15 MHz. At this situation , It is showing the Error in the clock configuration and when we select the option "Resolve clock issue Automatically" then the Clock becomes 120 MHz. Don't this protocol work in lower frequency?
In addition to that , I need to use SPI and FSMC in the same controller. Whether any issue will arise in future? Can anybody help me?