2023-04-30 06:43 AM
2023-04-30 09:09 AM
maybe you show some pic - so other people can see, what you talking about.
2023-04-30 09:28 AM
The "lively" colors are shown when you look at the chip from the bottom. Click the|..| button to flip the chip over.
2023-04-30 10:27 AM
Thank you... but ," Actually, the Flip horizontal/flip vertical buttons are available only for BGA packages." as ST say.
2023-04-30 05:16 PM
The pin outline is dashed when the pins actually cannot be seen and you are looking at them through the chip package.
2023-05-01 09:24 AM
Correct .... MX tries to give a physical representation of the micro, and in some cases the pins are 'hidden'. Thanks