cancel
Showing results for 
Search instead for 
Did you mean: 

In MX I noticed that the colors of the pins are, for some micros, more lively and the pins are drawn with solid lines, while in other cases with small strokes. (For example STM32F401RET and STM32F401CCUx). Am I making mistakes or is everything normal?

LVara.1
Associate II
 
5 REPLIES 5
AScha.3
Chief II

maybe you show some pic - so other people can see, what you talking about.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Evangelist III

The "lively" colors are shown when you look at the chip from the bottom. Click the|..| button to flip the chip over.

LVara.1
Associate II

Thank you... but ," Actually, the Flip horizontal/flip vertical buttons are available only for BGA packages." as ST say. ��

Piranha
Chief II

The pin outline is dashed when the pins actually cannot be seen and you are looking at them through the chip package.

Correct .... MX tries to give a physical representation of the micro, and in some cases the pins are 'hidden'. Thanks