cancel
Showing results for 
Search instead for 
Did you mean: 

I have and old STM32F429I-DISCO board, and I want to play with it with the CubeIDE 1.9.0, but that board is no more in the list, there is the new STM32F429I-DISC1 instead. What are the differences? How can I set-up the IDE to work with it properly?

ACont.1
Associate
 
2 REPLIES 2
TDK
Guru

The boards are largely the same. See here for differences:

https://community.st.com/s/question/0D53W00001PLKJtSAP/stm32cubemx-does-not-have-a-board-model-for-the-stm32f429idisc1-are-the-pinouts-for-the-disc1-the-same-as-the-disc

And here:

https://os.mbed.com/platforms/ST-Discovery-F429ZI/

If you feel a post has answered your question, please click "Accept as Solution".

Basically the VCP

Can use SWV for debug communication channel​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..