cancel
Showing results for 
Search instead for 
Did you mean: 

I can't assign 'adc value' in main / function statement

lee_daeun
Associate

I can get the adc values, 

but I want to use that values in main statement,

so when I assign that with new variable, the value is always 0.

 

Also in the function(send_frame) statement, the value is always 0 (send_frame function in my code)

 

Actually, It does work last week, but I don't know why it doesn't work suddenly,,,,

 

 

 

You can just watch variables, function/main statements. (and send_frame function)

I'm using Controller Area Network(CAN)

This is my code ! Thanks for help !

 

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2021 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "math.h"
#include "string.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

CAN_HandleTypeDef hcan1;

TIM_HandleTypeDef htim6;

/* USER CODE BEGIN PV */
HAL_StatusTypeDef ret;

/* TIMER6 Variables */
uint32_t  time_1ms;
uint32_t  Tim6_Flag_1ms;
uint32_t  Tim6_Flag_2ms;
uint32_t  Tim6_Flag_10ms;
uint32_t  Tim6_Flag_500ms;

/* CAN Variables */
CAN_FilterTypeDef sFilterConfig;
CAN_TxHeaderTypeDef TxHeader;
uint8_t TxData[8];
uint8_t RxData[8];
uint32_t TxMailbox;
uint8_t data_set1[8], data_set2[8], data_set3[8];
uint16_t CAN_ID[3] = {0x10, 0x11, 0x12};


/* EMG Variables */
uint16_t emg[5];
uint16_t good[5];
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_CAN1_Init(void);
static void MX_TIM6_Init(void);
static void MX_ADC1_Init(void);
/* USER CODE BEGIN PFP */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim);
HAL_StatusTypeDef CAN_Setting(void);
static void Can_FilterConfig(CAN_FilterTypeDef* sFilterConfig, uint32_t FilterBank, uint32_t FilterMode, uint32_t FilterScale, 
uint32_t FilterIdHigh, uint32_t FilterIdLow, uint32_t FilterMaskIdHigh, uint32_t FilterMaskIdLow, uint32_t FilterFIFOAssignment,
uint32_t FilterActivation, uint32_t SlaveStartFilterBank);
void CAN_CMD_STD(uint16_t id, uint8_t length, uint8_t* data);
void send_frame(void);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_DMA_Init();
  MX_CAN1_Init();
  MX_TIM6_Init();
  MX_ADC1_Init();
  /* USER CODE BEGIN 2 */
	HAL_TIM_Base_Start_IT(&htim6);	
	while(CAN_Setting() != HAL_OK){};
	HAL_Delay(500);
	HAL_ADC_Start_DMA(&hadc1, (uint32_t*) emg, 5);
good[0] = emg[0];

  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
		
		
		send_frame();
		/* 250HZ LOOP */

		
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 336;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 7;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief ADC1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_ADC1_Init(void)
{

  /* USER CODE BEGIN ADC1_Init 0 */

  /* USER CODE END ADC1_Init 0 */

  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC1_Init 1 */

  /* USER CODE END ADC1_Init 1 */

  /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
  */
  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV8;
  hadc1.Init.Resolution = ADC_RESOLUTION_12B;
  hadc1.Init.ScanConvMode = ENABLE;
  hadc1.Init.ContinuousConvMode = ENABLE;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
  hadc1.Init.NbrOfConversion = 5;
  hadc1.Init.DMAContinuousRequests = ENABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  if (HAL_ADC_Init(&hadc1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
  */
  sConfig.Channel = ADC_CHANNEL_11;
  sConfig.Rank = 1;
  sConfig.SamplingTime = ADC_SAMPLETIME_56CYCLES;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
  */
  sConfig.Channel = ADC_CHANNEL_12;
  sConfig.Rank = 2;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
  */
  sConfig.Channel = ADC_CHANNEL_13;
  sConfig.Rank = 3;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
  */
  sConfig.Channel = ADC_CHANNEL_14;
  sConfig.Rank = 4;
  sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
  */
  sConfig.Channel = ADC_CHANNEL_15;
  sConfig.Rank = 5;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC1_Init 2 */

  /* USER CODE END ADC1_Init 2 */

}

/**
  * @brief CAN1 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_CAN1_Init(void)
{

  /* USER CODE BEGIN CAN1_Init 0 */

  /* USER CODE END CAN1_Init 0 */

  /* USER CODE BEGIN CAN1_Init 1 */

  /* USER CODE END CAN1_Init 1 */
  hcan1.Instance = CAN1;
  hcan1.Init.Prescaler = 7;
  hcan1.Init.Mode = CAN_MODE_NORMAL;
  hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
  hcan1.Init.TimeSeg1 = CAN_BS1_15TQ;
  hcan1.Init.TimeSeg2 = CAN_BS2_8TQ;
  hcan1.Init.TimeTriggeredMode = DISABLE;
  hcan1.Init.AutoBusOff = ENABLE;
  hcan1.Init.AutoWakeUp = ENABLE;
  hcan1.Init.AutoRetransmission = ENABLE;
  hcan1.Init.ReceiveFifoLocked = DISABLE;
  hcan1.Init.TransmitFifoPriority = DISABLE;
  if (HAL_CAN_Init(&hcan1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN CAN1_Init 2 */

  /* USER CODE END CAN1_Init 2 */

}

/**
  * @brief TIM6 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_TIM6_Init(void)
{

  /* USER CODE BEGIN TIM6_Init 0 */

  /* USER CODE END TIM6_Init 0 */

  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM6_Init 1 */

  /* USER CODE END TIM6_Init 1 */
  htim6.Instance = TIM6;
  htim6.Init.Prescaler = 83;
  htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim6.Init.Period = 999;
  htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM6_Init 2 */

  /* USER CODE END TIM6_Init 2 */

}

/**
  * Enable DMA controller clock
  */
static void MX_DMA_Init(void)
{

  /* DMA controller clock enable */
  __HAL_RCC_DMA2_CLK_ENABLE();

  /* DMA interrupt init */
  /* DMA2_Stream0_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);

}

/**
  * @brief GPIO Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
/* TIMER setting */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
	
	if(htim->Instance == htim6.Instance) time_1ms++;
	if((time_1ms % 1) == 0) Tim6_Flag_1ms = 1;
	if((time_1ms % 2) == 0) Tim6_Flag_2ms = 1;
	if((time_1ms % 10) == 0) Tim6_Flag_10ms = 1;
	if((time_1ms % 500) == 0) Tim6_Flag_500ms = 1;
	
}

/* CAN Setting */
HAL_StatusTypeDef CAN_Setting(void)
{
	
	Can_FilterConfig(&sFilterConfig, 0, CAN_FILTERMODE_IDLIST, CAN_FILTERSCALE_16BIT, 0x10, 0x11, 0x12, 0x13, CAN_FILTER_FIFO0, ENABLE, 14);
	if (HAL_CAN_Start(&hcan1) != HAL_OK)
  {
    /* START ERROR */
    Error_Handler();
  }
	if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
  {
    /* NOTIFICATION ERROR */
    Error_Handler();
  }
	if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING) != HAL_OK)
  {
    /* NOTIFICATION ERROR */
    Error_Handler();
  }
	return HAL_OK;
	
}

/* CAN FILTER Setting */
static void Can_FilterConfig(CAN_FilterTypeDef* sFilterConfig, uint32_t FilterBank, uint32_t FilterMode, uint32_t FilterScale, 
uint32_t FilterIdHigh, uint32_t FilterIdLow, uint32_t FilterMaskIdHigh, uint32_t FilterMaskIdLow, uint32_t FilterFIFOAssignment,
uint32_t FilterActivation, uint32_t SlaveStartFilterBank)
{	
  
	sFilterConfig->FilterBank = FilterBank;
  sFilterConfig->FilterMode = FilterMode;
  sFilterConfig->FilterScale = FilterScale;
	sFilterConfig->FilterIdHigh = FilterIdHigh<<5;
  sFilterConfig->FilterIdLow = FilterIdLow<<5;
  sFilterConfig->FilterMaskIdHigh = FilterMaskIdHigh<<5;
  sFilterConfig->FilterMaskIdLow = FilterMaskIdLow<<5;
  sFilterConfig->FilterFIFOAssignment = FilterFIFOAssignment;
  sFilterConfig->FilterActivation = FilterActivation;
  sFilterConfig->SlaveStartFilterBank = SlaveStartFilterBank;
	if(HAL_CAN_ConfigFilter(&hcan1, sFilterConfig) != HAL_OK)
  {
		/* Filter Configuration Error */
    Error_Handler();
  }
	
}

// CAN trasmission

void CAN_CMD_STD(uint16_t id, uint8_t length, uint8_t* data)
{
	
  int k=0;	
	
	TxHeader.StdId = id;
  TxHeader.DLC = length;
  TxHeader.RTR = CAN_RTR_DATA;
  TxHeader.IDE = CAN_ID_STD;
	TxHeader.TransmitGlobalTime = DISABLE;
		
	for ( k = 0 ; k < length ; k ++ ) TxData[k] = data[k];
	
	if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK)
  {
          /* Transmission request Error */
          Error_Handler();
  }
	
	while(HAL_CAN_GetTxMailboxesFreeLevel(&hcan1) != 3) {}; //Wait transmission complete
		
}

void send_frame()
{
	// FSR
	data_set1[0] = emg[0];
	data_set1[1] = (emg[0]>>8);
	data_set1[2] = emg[1];
	data_set1[3] = (emg[1]>>8);
	data_set1[4] = emg[2];
	data_set1[5] = (emg[2]>>8);
	data_set1[6] = emg[3];
	data_set1[7] = (emg[3]>>8);
	
	// Load cell
	data_set2[0] = emg[4];
	data_set2[1] = (emg[4]>>8);
	
	//data_set2[2] = adc_val[5];
	//data_set2[3] = (adc_val[5]>>8);
	
	// angle conversion
	//memcpy(&ang_u32[0],&ang[0],8);
	//memcpy(&ang_u32[1],&ang[1],8);
	/*
	data_set3[0] = ang_u32[0];
	data_set3[1] = (ang_u32[0]>>8);
	data_set3[2] = (ang_u32[0]>>16);
	data_set3[3] = (ang_u32[0]>>24);
	data_set3[4] = ang_u32[1];
	data_set3[5] = (ang_u32[1]>>8);
	data_set3[6] = (ang_u32[1]>>16);
	data_set3[7] = (ang_u32[1]>>24);
	*/
	//Transmission
	CAN_CMD_STD(CAN_ID[0], 8, data_set1);
	CAN_CMD_STD(CAN_ID[1], 8, data_set2);
	CAN_CMD_STD(CAN_ID[2], 8, data_set3);
}



/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
1 REPLY 1

Probably duplicate