‎2019-04-02 10:20 AM
Hello
I am using :
I already created the files
when i use f_mount i get FR_NO_FILESYSTEM
thx
Solved! Go to Solution.
‎2019-04-03 9:49 AM
Capacity seems all wrong for a 4GB eMMC, and I'm not sure I've coded to manage anything below 2GB
The ODROID cards with their MicroSD adapter connect more directly into the STM32 DISCO/EVAL boards.
‎2019-04-02 11:10 AM
>>when i use f_mount i get FR_NO_FILESYSTEM
Blank eMMC devices will need to be formatted. If you've validated the READ, and then WRITE functionality, you're ready to use f_mkfs()
I found these ODROID cards to be less of a circus
https://www.hardkernel.com/shop/8gb-emmc-module-c2-android/
‎2019-04-02 3:38 PM
STM32F413H-DISCO eMMC test code, blind port, I don't own this board.
Outputs via VCP at 115200 8N1, at first prompt hit ENTER, will prompt to format if necessary.
‎2019-04-03 8:22 AM
Thank you for your reply. I tried your source code it happens to connect with the eMMC but it can neither write nor erase. I tested it with several eMMCs always the same thing in the attached file you find all msg.
‎2019-04-03 9:49 AM
Capacity seems all wrong for a 4GB eMMC, and I'm not sure I've coded to manage anything below 2GB
The ODROID cards with their MicroSD adapter connect more directly into the STM32 DISCO/EVAL boards.
‎2019-04-09 7:20 AM
Hello @Community member​
Thanks for all the valuable. We solved the problem and all seems correct now.
‎2023-08-22 8:39 AM
Do you have stm32f4 emmc 5.1 example working with iNAND 7250 ?
‎2023-09-30 4:20 AM
Hello dear Mcherif
I have a similar challenge to you
Would it be possible to explain and post a sample code where FATFS is implemented via SDIO on EMMC memory.
‎2023-12-05 12:58 AM
I'd also be interested in your outcome especially of the FATFS... It would be nice to have a list of things working and the code that goes along with it. It might also be interesting for future users if it is only for reference...