Skip to main content
Associate III
March 13, 2024
Solved

How to know if there are any memory directions reserved?

  • March 13, 2024
  • 7 replies
  • 1860 views

Hello!

I am trying to use DTCMRAM on my stm32h743zi micro.

When i use an array located from 0x20001760 to 0x200017d4 there are some positions that do not update, it stays in 0 or "inf" value, but when i use other array located in different location, it works perfectly.

My question is..., Is there any reserved directions in this memory that are not allowed to use?  If yes, how can i know which positions i can not use?

 

Thank you so much to everybody!

This topic has been closed for replies.
Best answer by TDK

If they're not 0, something probably wrote to them and you're seeing the result. Perhaps initialize the array to known values before it is used.

Reduce your code to a minimal example to convince yourself that memory is working as expected.

7 replies

TDK
March 13, 2024

There aren't any reserved locations. You should be able to read and write wherever you want in DTCM.

Typically, memory values are 0x00 or 0xFF when not initialized. Where is it showing "inf"? Probably there is some other explanation for what you are seeing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
ST Technical Moderator
March 13, 2024

Hello,

Nothing prevents you to use the overall DTCM memory (128 Kbytes).

Maybe you need to provide more information of your context: Which IDE? how are you accessing the DTCM RAM? Show some screenshots, etc .. Maybe also to share your project?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
rubenlesAuthor
Associate III
March 13, 2024

Hi @TDK2 . I show you in the next image, there are a few values in 0 and then in "inf" using these directions. 

rubenles_1-1710337078973.png

But if i use other array with other directions, everything works perfectly. I am lost in this problem.

rubenles_2-1710337292589.png

 

Thank you so much

 

 

TDK
TDKBest answer
March 13, 2024

If they're not 0, something probably wrote to them and you're seeing the result. Perhaps initialize the array to known values before it is used.

Reduce your code to a minimal example to convince yourself that memory is working as expected.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
March 13, 2024

The problem is that you want to use uninitialized memory where you have not written any data. The C library zero-initializes only the "bss" memory defined in your program. If other memory areas should be zero-initialized, do it yourself.

Tesla DeLorean
Guru
March 13, 2024

The ST GNU startup.s code is a bit naive, would suggest code that explicitly clears other sections of memory that the linker/script dole out. You have to add code to copy initial content from FLASH, or clear.

Keil, IAR, and Arduino GNU do this better, with table driven methods.

Nothing is reserved in DTCMRAM, just be aware it's not cached, and optimization and volatile setting may impact how data is pushed back into memory, and seen by the debugger at certain points.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rubenlesAuthor
Associate III
March 14, 2024

Thanks @TDK @Tesla DeLorean @Pavel A. @mƎALLEm for all your answers.

I was looking for the issue and... I was using a variable that was overwriting some position of the array that I sent here..., indeed, the addresses can be fully used.

At least I have that information for the future... 

Thank you all for your time. Appreciate it.