2020-11-30 8:58 AM
If I tick the enable box in STM32CUBEMX the interrupt is enabled when MX_GPIO_Init() is executed. Since this is prior to the initialisation of FreeRTOS queues etc this turns into a disastrous mess.
If I leave the box unticked then everything assoociated with this interrupt must be written manually.
It's a shame that the interrupt can't be setup in the MX and then manually enabled when the appropriate FreeRTOS task becomes active.
Solved! Go to Solution.
2020-11-30 5:37 PM
No, it is not a shame, you just need to know the trick.
Insert the following line before the cube generated code that configures NVIC interrupts:
__set_BASEPRI(configMAX_SYSCALL_INTERRUPT_PRIORITY);This will disable all interrupts that should not occur before FreeRTOS scheduler starts.
When it starts and any thread runs, BASEPRI will automatically return to 0 and these interrupts will be unmasked.
And the life is good again =)
Note: assuming that priority of HAL timer interrupt is higher than SYSCALL_INTERRUPT_PRIORITY. The HAL tick is used to detect timeouts during initialization of many HAL drivers so it should normally work as soon as the HAL starts it.
-- pa
2020-11-30 12:34 PM
> If I leave the box unticked then everything assoociated with this interrupt must be written manually.
And why would that be a problem? It's a write to two or three registers, and then enabling the interrupt in NVIC. Hardly a challenge.
Cube/CubeMX inevitably caters only for a limited subset of the virtually infinite modes of usage of the peripherals. There's just so many things you can control by clicking. I'm sure ST is willing to provide you a dedicated clicking interface for whatever functionality you desire, if you present a significant buying power (as expressed in $M+).
JW
2020-11-30 5:37 PM
No, it is not a shame, you just need to know the trick.
Insert the following line before the cube generated code that configures NVIC interrupts:
__set_BASEPRI(configMAX_SYSCALL_INTERRUPT_PRIORITY);This will disable all interrupts that should not occur before FreeRTOS scheduler starts.
When it starts and any thread runs, BASEPRI will automatically return to 0 and these interrupts will be unmasked.
And the life is good again =)
Note: assuming that priority of HAL timer interrupt is higher than SYSCALL_INTERRUPT_PRIORITY. The HAL tick is used to detect timeouts during initialization of many HAL drivers so it should normally work as soon as the HAL starts it.
-- pa
2020-11-30 6:00 PM
Yes I appreciate it can't be the singing and dancing solution for everyone all the time. But when FreeRTOS is used, where queues are typically filled from interrupts it becomes a certain failure for anyone using FreeRTOS.
2020-11-30 6:35 PM
I can see the significance of your note. The current priority set by the FreeRTOS middleware is now 15. Until the latest version of MX it was 0, so unmaskable. I have no idea why the change but of course it does mean that HAL_Delay no longer works.
2020-11-30 7:03 PM
In the end I used the following lines:
HAL_InitTick(0);
__set_BASEPRI(configMAX_SYSCALL_INTERRUPT_PRIORITY);
Many thanks for your help.