2023-08-29 1:10 AM
hi all,
Why does the system crash when registering an initialized display driver using lv_disp_drv_register() within “In Register” section? how to replace lv_hal_disp.c for freertos.
1
lv_memset_00(disp, sizeof(lv_disp_t))
After executing the lv_memset_00(disp, sizeof(lv_disp_t)) statement, set the free BlockSize in the BlockLink_t structure to 0 (zero).
then Insert the new block into the list of free blocks (prvInsertBlockIntoFreeList( ( pxNewBlockLink ) )) Due to sufficient space (as subtracting any number from 0 results in a negative number, i.e., a large number), it enters an infinite loop.
2.Create a refresh timer
lv_timer_create(_lv_disp_refr_timer, LV_DISP_DEF_REFR_PERIOD, disp);
why it Add a new head to a linked list to create timer task ?
FreeRTOS Kernel V10.3.1, use heap_4.c
LVGL V8.0.0
board stm32h743
add pvPortRealloc() at heap_4.c
```c
void *pvPortRealloc(void *mem, size_t newsize) { if (newsize == 0) { vPortFree(mem); return NULL; } void *p; p = pvPortMalloc(newsize); if (p) { /* zero the memory */ if (mem != NULL) { memcpy(p, mem, newsize); vPortFree(mem); } } return p; }
```
2023-08-29 1:22 AM
You should probably increase the TOTAL_HEAP_SIZE in memory management in your RTOS setting and also the Stack size for your task.
2023-08-29 1:41 AM
hi Slh,
thank your reply.
i have been adjust increase the "heap size", but when
lv_memset_00(disp, sizeof(lv_disp_t)) // clear lvgl handle struct
After executing the lv_memset_00(disp, sizeof(lv_disp_t)) statement, set the free BlockSize in the BlockLink_t structure to 0 (zero). So ,it not found node to insert or clear free BlockLink size.
```c
lv_disp_t * lv_disp_drv_register(lv_disp_drv_t * driver)
{
lv_disp_t * disp = _lv_ll_ins_head(&LV_GC_ROOT(_lv_disp_ll));
LV_ASSERT_MALLOC(disp);
if(!disp) {
return NULL;
}
/*Create a draw context if not created yet*/
if(driver->draw_ctx == NULL) {
lv_draw_ctx_t * draw_ctx = lv_mem_alloc(driver->draw_ctx_size);
LV_ASSERT_MALLOC(draw_ctx);
if(draw_ctx == NULL) return NULL;
driver->draw_ctx_init(driver, draw_ctx);
driver->draw_ctx = draw_ctx;
}
// reset BlockLink_t
lv_memset_00(disp, sizeof(lv_disp_t));
disp->driver = driver;
disp->inv_en_cnt = 1;
lv_disp_t * disp_def_tmp = disp_def;
disp_def = disp; /*Temporarily change the default screen to create the default screens on the
new display*/
/*Create a refresh timer*/
// assign invaild value at BlockLink_t struct
disp->refr_timer = lv_timer_create(_lv_disp_refr_timer, LV_DISP_DEF_REFR_PERIOD, disp);
LV_ASSERT_MALLOC(disp->refr_timer);
if(disp->refr_timer == NULL) {
lv_mem_free(disp);
return NULL;
}
if(driver->full_refresh && driver->draw_buf->size < (uint32_t)driver->hor_res * driver->ver_res) {
driver->full_refresh = 0;
LV_LOG_WARN("full_refresh requires at least screen sized draw buffer(s)");
}
disp->bg_color = lv_color_white();
#if LV_COLOR_SCREEN_TRANSP
disp->bg_opa = LV_OPA_TRANSP;
#else
disp->bg_opa = LV_OPA_COVER;
#endif
#if LV_USE_THEME_DEFAULT
if(lv_theme_default_is_inited() == false) {
disp->theme = lv_theme_default_init(disp, lv_palette_main(LV_PALETTE_BLUE), lv_palette_main(LV_PALETTE_RED),
LV_THEME_DEFAULT_DARK, LV_FONT_DEFAULT);
}
else {
disp->theme = lv_theme_default_get();
}
#endif
disp->act_scr = lv_obj_create(NULL); /*Create a default screen on the display*/
disp->top_layer = lv_obj_create(NULL); /*Create top layer on the display*/
disp->sys_layer = lv_obj_create(NULL); /*Create sys layer on the display*/
lv_obj_remove_style_all(disp->top_layer);
lv_obj_remove_style_all(disp->sys_layer);
lv_obj_clear_flag(disp->top_layer, LV_OBJ_FLAG_CLICKABLE);
lv_obj_clear_flag(disp->sys_layer, LV_OBJ_FLAG_CLICKABLE);
lv_obj_set_scrollbar_mode(disp->top_layer, LV_SCROLLBAR_MODE_OFF);
lv_obj_set_scrollbar_mode(disp->sys_layer, LV_SCROLLBAR_MODE_OFF);
lv_obj_invalidate(disp->act_scr);
disp_def = disp_def_tmp; /*Revert the default display*/
if(disp_def == NULL) disp_def = disp; /*Initialize the default display*/
lv_timer_ready(disp->refr_timer); /*Be sure the screen will be refreshed immediately on start up*/
return disp;
}
```
```c
lv_timer_t * lv_timer_create(lv_timer_cb_t timer_xcb, uint32_t period, void * user_data)
{
lv_timer_t * new_timer = NULL;
new_timer = _lv_ll_ins_head(&LV_GC_ROOT(_lv_timer_ll));
LV_ASSERT_MALLOC(new_timer);
if(new_timer == NULL) return NULL;
new_timer->period = period;
new_timer->timer_cb = timer_xcb;
new_timer->repeat_count = -1;
new_timer->paused = 0;
new_timer->last_run = lv_tick_get();
new_timer->user_data = user_data;
timer_created = true;
return new_timer;
}
LV_ATTRIBUTE_FAST_MEM void lv_memset_00(void * dst, size_t len)
{
uint8_t * d8 = (uint8_t *)dst;
uintptr_t d_align = (lv_uintptr_t) d8 & ALIGN_MASK;
/*Make the address aligned*/
if(d_align) {
d_align = ALIGN_MASK + 1 - d_align;
while(d_align && len) {
SET8(0);
len--;
d_align--;
}
}
uint32_t * d32 = (uint32_t *)d8;
while(len > 32) {
REPEAT8(SET32(0));
len -= 32;
}
while(len > 4) {
SET32(0);
len -= 4;
}
d8 = (uint8_t *)d32;
while(len) {
SET8(0);
len--;
}
}
```