cancel
Showing results for 
Search instead for 
Did you mean: 

EXAMPLE for H7R with bad .ioc

mbarg.1
Lead

in LwIP_UDPTCP_Echo_Server_Netconn_RTOS example for H7S3, 

LwIP_UDPTCP_Echo_Server_Netconn_RTOS.ioc returns error 

Invalid State: Most probably trying to open 'LwIP_UDPTCP_Echo_Server_Netconn_RTOS.ioc' file from an abnomal previous IDE session exit. Please close such editor and have a new try to recover properly.

but there are no other editors open - i just downloaded a fresh version in new directory.

Using STM32CubeIde 1.8.1 in Window computer

Opening 

6 REPLIES 6
Saket_Om
ST Employee

Hello @mbarg.1 

I opened it on my side it works correctly. Please use the latest version of CubeMX.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

I have version 1.18.1 - same problem with windows and linux debian - updated 2 days ago

What is the CubeMX version ?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

Cube MX

Version: 6.14.1-RC5

Build: 20250409-1515 (UTC)

 

STM32CubeIDE

 

Version: 1.18.1

Build: 24813_20250409_2138 (UTC)

TDK
Super User

Opens fine here in standalone CubeMX.

How are you trying to open it in CubeIDE? File -> New -> From existing IOC?

If you feel a post has answered your question, please click "Accept as Solution".

In STM32CubeIde, I made File-> New->STM32 project, than selected Examples, H7R, and LwIP_UDPTCP_Echo_Server_Netconn_RTOS .

When I open LwIP_UDPTCP_Echo_Server_Netconn_RTOS.ioc, I get this error.