2019-01-14 4:02 AM
I have created sample code for STM32L010R8 using cubemx v5.0.1. When I try to compile the code, I am getting this error. What couldbe the reason.
Please help.
2019-01-14 4:34 AM
An incorrect library ?
The Cortex M0/M0+ supports only a subset of thumb instructions, so linking against M3/M4 libs will fail.
I don't use Cube, not sure what role it plays here in connection with your toolchain.
2020-01-16 12:41 AM
I have the same issue. Its the same every time you update the CUBE it makes working projects stop working. I wish they would test or leave things alone. If its not broke do not fix it.
Description Resource Path Location Type
make: *** [Drivers/STM32F1xx_HAL_Driver/Src/stm32f1xx_hal_cortex.o] Error 1 AQU83 C/C++ Problem
selected processor does not support `dsb 0xF' in Thumb mode AQU83 line 292, external location: C:\Users\Ricky\AppData\Local\Temp\ccjy6QCz.s C/C++ Problem
selected processor does not support `dsb 0xF' in Thumb mode AQU83 line 345, external location: C:\Users\Ricky\AppData\Local\Temp\ccjy6QCz.s C/C++ Problem
selected processor does not support `dsb 0xF' in Thumb mode AQU83 line 367, external location: C:\Users\Ricky\AppData\Local\Temp\ccjy6QCz.s C/C++ Problem
selected processor does not support `isb 0xF' in Thumb mode AQU83 line 303, external location: C:\Users\Ricky\AppData\Local\Temp\ccjy6QCz.s C/C++ Problem
Still no solution posted ?
2020-01-16 1:07 AM
The DSB instruction requires ARMv7 (M3 and up), the M0/M0+ is ARMv6.
It seems CubeMX mostly increases in size and number of supported devices, but not much in quality and robustness.
2020-01-16 4:19 AM
I have re-installed 64 bit Java, reinstalled the whole SW4STM32.... Still the same issue.
All I want to do is change the function of 3 pins to GP Outputs.
Using the cube to generate the code just breaks it. Compiles OK before that (Old project).
The issue is compiling stm32f1xx_hal_cortex.c
If I comment out the HAL_CORTEX_MODULE_ENABLED these errors go away but I get a bunch of others. I do not think this update was tested.
I will just write to the registers to set the IO up and just forget about the CUBE. What a joke!
2020-01-16 4:37 AM
> The issue is compiling stm32f1xx_hal_cortex.c
This seems strange. The F1xx devices are Cortex M3, and do support DSB/ISB instructions.
I might mention I'm no Cube user, for certain unnamed reasons.
2020-02-06 3:59 PM
Guys, look carefully at the error - the instruction has an option "0xF". That is only supported in full ARM instruction set, but not in Thumb mode on Cortex-M3. The compiler is missing -mcpu=cortex-m3 parameter.
https://lmgtfy.com/?q=Error%3A+selected+processor+does+not+support+%60dsb+0xF%27+in+Thumb+mode
2021-03-12 9:29 AM
hello Piranha , where to add -mcpu=cortex-m3 parameter in Cube IDE ?
thanks
2021-06-02 1:25 AM
Hi, I had the same error, and found out you can add the "-mcpu=cortex-m4" flag in the "Miscellaneous" tab :