2020-06-03 03:47 AM
2020-06-03 05:38 AM
Hello Hicss.2033,
STM32CubeMx covers the whole portfolio of STM32 microcontrollers, based on 32-bit Arm Cortex cores. It allows configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core.
It is available as standalone software running on Windows®, Linux® and macOS® (macOS is a trademark of Apple Inc. registered in the U.S. and other countries.) operating systems, or through Eclipse plug-in.
For more details check: https://www.st.com/en/development-tools/stm32cubemx.html.
FreeRTOS™ is the class of RTOS is used to run on STM32 microcontroller or microprocessor. For more details please refer to the UM of Developing applications on STM32Cube with RTOS: https://www.st.com/resource/en/user_manual/dm00105262-developing-applications-on-stm32cube-with-rtos-stmicroelectronics.pdf
Best Regards,
Khouloud.