cancel
Showing results for 
Search instead for 
Did you mean: 

CubMX 6.5.0 ADC issue with STM32G0

bertram007
Associate

Hallo,

after Upgrading to CubeMX 6.5.0 there are problems using ADC1 with STM32G070RBT6. When the 'Number of Conversion' > 1 it is not possible to set 'Discontinuous Conversion Mode' to Disabled (only Enabled), with CubeMX 6.4.0 it works. Is this a bug?

1 REPLY 1

Hello @bertram007​,

Welcome to the STM32 Community and thanks for having reported.

To directly answer your question, yes this is an issue with the last STM32CubeMX version. It has been reported internally to be fixed as soon as possible.

I'll keep you posted with the updates.

A similar issue war reported by this post, please refer to it for further details.

Sorry for any inconvenience that this may cause.

Khouloud.