2020-03-30 6:26 AM
In the old standalone version of CubeMX one could access the datasheet/application notes appropriate to the board/CPU part your project was based on.
Probably me being a bit dense but I can't see to find this in CubeIDE. Does an equivalent exist?
Used to save a lot of time hunting for relevant documents.
Thanks
Pete
2020-03-31 2:45 AM
File > New STM32 Project
Let's select your device (mcu or board) then rely on dedicated button on same target selector page to get related doc.
2020-03-31 2:53 AM
Having to start a new project each time instead of just pressing Alt-D is a terrible workaround.
2020-03-31 5:07 AM
Yes i may agree but at least doing the job.
2020-03-31 5:37 AM
Thanks for the pointer, a bit of a kludge but better than nothing :) Be nice if the feature was extended in to a existing project though.