cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.14 generate OpenAMP error in STM32H747 error.

Tom17
Associate II

Hi all,

I am using CubeMX 6.14 to generate an OpenAMP project for the STM32H747I-DISCO board. When I build the project, I receive the following warnings, and it results in an 'OpenAMP create endpoint' error at runtime. I used the same code and project created with CubeMX 6.12, and it works fine. Therefore, I suspect there might be an issue with CubeMX 6.14. Could someone please advise me on how to generate a working OpenAMP project using CubeMX?

arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined <command-line>: note: this is the location of the previous definition arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rcc_ex.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined <command-line>: note: this is the location of the previous definition arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rtc.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined <command-line>: note: this is the location of the previous definition arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rtc_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_rtc_ex.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined <command-line>: note: this is the location of the previous definition arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined <command-line>: note: this is the location of the previous definition arm-none-eabi-gcc "D:/TouchGFXProjects/STM32H7_TUT/Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim_ex.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DUSE_HAL_DRIVER -DSTM32H747xx -DUSE_PWR_DIRECT_SMPS_SUPPLY -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DRPMSG_BUFFER_SIZE=512 -DVIRTIO_SLAVE_ONLY -DRPMSG_BUFFER_SIZE -DNO_ATOMIC_64_SUPPORT -c -I../../../CM4/Core/Inc -I../../../Drivers/BSP/Components -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/CMSIS/Include -I../../../CM4/OPENAMP -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include/metal/compiler/gcc -I../../../Middlewares/Third_Party/OpenAMP/open-amp/lib/rpmsg -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.d" -MT"Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_tim_ex.o" <command-line>: warning: "RPMSG_BUFFER_SIZE" redefined
1 ACCEPTED SOLUTION

Accepted Solutions
sirhc79
Associate

So there is a wrong (re)definition of RPMSG_BUFFER_SIZE in the project settings. A temporary solution is to remove it from the project settings for both cores and recompile. 

sirhc79_0-1745230283786.png

Regards, 

Chris

 

View solution in original post

8 REPLIES 8
Ghofrane GSOURI
ST Employee

Hello @Tom17 

First let me thank you for posting.

I'm currently checking this issue internally,  I will get back to you asap.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Kenwang
Associate III

Hi Ghofrane,

I also encountered the same problem, is there a solution to this problem?

Ghofrane GSOURI
ST Employee

Hello @Tom17 

Issue has been raised to dev team .

Internal ticket number : 207197

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

NickO
Associate III

Same for Cube IDE v1.18

Hi @Ghofrane GSOURI ,

Since my project is quite urgent, I was wondering if you could provide a workaround or a method for manual modification?

Tom17
Associate II

This bug is still present in version 6.14.1 and hasn't been resolved. Is there a plan to fix it?

sirhc79
Associate

So there is a wrong (re)definition of RPMSG_BUFFER_SIZE in the project settings. A temporary solution is to remove it from the project settings for both cores and recompile. 

sirhc79_0-1745230283786.png

Regards, 

Chris

 

Tom17
Associate II

Hi Chris,

Thank you for your explanation. The issue has been resolved.