cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 5.1 - CMSIS DSP library missing for Toolchain SW4STM32

Max Rest
Associate II

Hello STM,

when I generate a project for STM32H750 with CubeMX 5.1 with Toolchain SW4STM32 selected, CMSIS DSP library is missing from the project and it does not compile.

Also, a preprocessor define of

__ARM_ARCH_7EM__=1

is missing to specify the ARM Architecture, which leads to missing gcc intrinsics in cmsis_gcc like __SSAT and the likes.

1 REPLY 1

Use Keil uVision is better for STM32 programming