2017-01-11 11:34 PM
hi
I'm using CubeMX 4.18.0 recently.
by the way,
Every time An error occurs when creating a TrueStudio project using the CubeMX 4.18.0.
Please, help.
Solved! Go to Solution.
2017-02-17 2:18 AM
Hi,
This issue is already resolved based on this discussion
https://community.st.com/0D50X00009XkeisSAB
Regards
Imen
2017-01-12 12:27 AM
Hi,
Which version of
TrueStudio using ? Make sure to use the last version.
Maybe this is due to a long path issue. So, try to change with the short path. Do a clean then rebuild and import to
TrueStudio
.Please keep us informed on your progress
.
2017-01-12 1:34 AM
TrueStudio version is 7.0.1.
This is latest version of TrueStudio.
thanks.
2017-01-12 1:43 AM
and,
Because of this problem, I was able to format the my Computer and install new TrueStudio 7.0.1
and CubeMX 4.18.0, but I could not solve the error.
2017-01-12 1:58 AM
Long path problem.
Creating a project on a desktop created normally.
However, long path problem should be solved.
thanks.
2017-01-12 2:23 AM
After modifying a project created by another cubemx version of the projects,
the same error occurs after regenerating the code.
2017-01-12 2:48 AM
Hi
SoHaeng.Lee
,This issue is reported to CubeMx team formore investigation.
Keep us informed about your feedback, this will help our team tomore understand the issue you are facing.
Regards
-ID-
2017-01-15 7:02 PM
Hi
After updating cubemx to 4.19.0, the problem has been resolved.
I'll give feedback through more tests.
Thank you for developing the cubemx Development team.
2017-01-29 7:29 AM
The error occurred in 4.18.0 CubeMX, also known as CubeMX 4.19.0.
I'd like to attach a project file, so what should I do?
target mcu : stm32f103c8t6
compiler : TrueStudio 7.0.1
CubeMX : 4.19.0
2017-01-29 8:04 AM
Not sure you can add attachments to comments. You might be able to edit your original top post to add them, and of course you can use things like DropBox or Google Drive and provide links.