cancel
Showing results for 
Search instead for 
Did you mean: 

Cube MX and Flash

tekampe
Associate II
Posted on August 11, 2016 at 08:17

Hey,

i'm using CubeMX to generate code. In one of the examples is an EEPROM emulation (STM32Cube_FW_F1_V1.4.0\Projects\STM32F103RB-Nucleo\Applications\EEPROM\EEPROM_Emulation) which I want to use. 

My Problem is that I can not find the Button in CubeMX so that the generated stm32f1xx_hal_conf.h enables the HAL_FLASH_MODULE_ENABLED define.

I hope you can help me.

Jens

#cubemx-hal-flash
1 REPLY 1
Nesrine M_O
Lead II
Posted on August 11, 2016 at 11:30

Hi Jens,

The flash is enabled by default using CUMEMX.

-Syrine-