2022-10-25 5:57 AM
I am trying to port C libraries I made using LL Libraries generated from STM32CubeMX to C++ under STM32CubeIDE and I am looking for advice on how to accomplish the following:
I Created and object wich uses USART_LL Libraries and wanted to have something simillar to:
#include "main.h"
#include "stm32l1xx_it.h"
#include "object_lib.h"
extern object_type object;
void USART1_IRQHandler(void)
{
object.usart_ISR();
}But since the it file is a "C" one I cannot use this OOP style.
So I've beeng thinking about creating a wrapper-like structure so I can call one function with no parameters where somehow the ISR will be called, but I got the feel the implementation won't be as portable as I would like considering we always stepped aside from dynamic memory allocation.
//On interrupt C File
#include "main.h"
#include "stm32l1xx_it.h"
#include "object_lib.h"
void USART1_IRQHandler(void)
{
object_isr_wrapper();
}
//On object_lib.h
#include "main.h"
#include "uart_LL.h"
#pragma once
#ifdef __cplusplus
extern "C"{
#endif
void object_isr_wrapper();
#ifdef __cplusplus
}
//On object_lib.cpp
class Object{
...
};
Object object;
Object object_list = {&object};
void object_isr_wrapper(){
for(every_object...){
object_list[index]->isr();
}
}Ideally I would like to use OOP wherever I can as my objective is to port everything to C++ but I am still unaware of all the musts and dont's when using the STMCubeMX C generated libraries in this context.
Maybe I sould just go with dyncamic memory allocation so I don't have to manually fill the array on static memory... Maybe should I stop and continue with C before I get too far?... Any advice will be much appreciated.
Thanks, VL.
2022-10-25 8:17 AM
Couldn't you just have the handler code in IT.CPP or similar?
That way the name mangling and linkage/binding would work directly out of the vector table.
2022-10-25 9:21 AM
> Maybe should I stop and continue with C before I get too far?.
That's a good idea too.
2022-11-09 10:48 AM
I decided for this,
I'd rather work with C as it is fully supported on STM32CubeIDE, everything is generated in C and the logic behind how things works just keeps making sense in C :)