cancel
Showing results for 
Search instead for 
Did you mean: 

Identifying updatable items in the bundles manager

AHugh.2
Associate III

Hi,

In the bundles manager for my project is it possible to view at a glance items where there is an update available? Currently the status column icon doesn't differentiate between updatable items - only when I open the version drop-down does it become clear there are newer version(s) available (or I select all then hover over the update button).

Also, same goes for "cube pack list" command - can this show a list of updatable items?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
vincent_grenet
ST Employee

@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.

View solution in original post

4 REPLIES 4
Cartu38 OpenDev
Lead III

Status column is right one and sortable. Variation is thin but exists. Check icon is not exactly same. One is negative of the second. Looks at it carefully.

Way to update them all thanks VSCode integrated terminal is 'cube bundle update'

I've not found way to list updatable for packs. Here way to sync. is 'cube pack sync'

If you look at the "System" bundles manager then yes, there is a difference in the icon, but in the project one there is not.

AHugh2_1-1754551877081.png

So here, 1.0.0 is bold and selected indicating it is the current one, but there is a newer 1.0.1 one, but the icon in the status column is indentical as far as I see.

Very minor point!

vincent_grenet
ST Employee

@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.

vincent_grenet
ST Employee

Please be aware that stm32cube-ide-bundles-manager-0.23.3.vsix has been released to address reported concerns.