2025-03-10 3:31 AM
I installed stm32CubeIDE version 1.18.0
Started a new stm32 project, selected my board, clicked ok for everything (like it showed a window which contained 5 checked options of led,virtual port etc etc.), i selected all and clicked ok.
Then activated XCubeAI package, checked core and selected validation under application, then clicked on OK.
Then i tried to open that network window... but before that a small window opened which showed configuring usart3 and it got stuck at 70% for very long time... i tried closing the app and disconnecting, restarting pc... but the same thing is happening... i shared a screenshot of where it got stuck...
PLease help me with this...
2025-03-10 3:53 AM
Did it run ok before enabling AI package?
2025-03-10 3:59 AM
I didnot run anything before that... i directly started a new stm32 project and enabled ai package and tried to add .onnx file.. but it showed that and got stuck there
2025-03-10 6:14 AM
I didnot run anything before that... i directly started a new stm32 project and enabled ai package and tried to add .onnx file.. but it showed that and got stuck there
Should i change anything there????
2025-03-10 7:07 AM
PLease respond....
2025-03-10 7:36 AM - edited 2025-03-10 7:37 AM
My suggestion is:
I did this and I got no problems - should be some difference between my and your project.
Unless you post your project or at least .ioc, it will be difficult to help you...
Remembeer to remove Debug dir before posting !
2025-03-10 7:41 AM
Actually... i tried restarting it multiple times...
And i am in my first step... i didnt even added my network there... the first stage itself is the problem....
Can you please specify it in more detailed way... please
2025-03-10 9:58 PM
2025-03-10 11:17 PM
Again:
Another question: are you logged off or using a VPN? STM32CubeIde does not work (sometime) if you are not logged and on a direct connection, probably copyright issues.
2025-03-11 10:51 AM
There are soo many errors and warnings...
I think by default, nucleo-h753zi board's stlink is directed to usart3??
but in my connectivity tab at cubeMX, usart3 is not even available... i am not even trying to enable it... please try to help.... it is fine until validation on desktop.. but when i try to build and compile... it is not happening...