2024-06-11 9:41 PM
Hello ,, can anyone share the code for generated with cubeMX version 6.1.0 and above. ethernet with udp pinging works code . the code should able to run in keil... thanks.....
2024-06-12 12:28 AM - edited 2024-06-12 12:30 AM
Hello @ramsita ,
There is no .ioc files (ready for use project) with CubeMX.
Ready-to-use UDP applications running in keil can be found in the STM32CubeH7 MCU package:
This ST wiki page may help you to create project from scratch:
How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community