2023-04-17 01:56 AM - edited 2023-11-20 07:57 AM
As you can see here, the bottum tab of MDMA tab window, has bot been loaded and the MX tab does not respond.
I have to close the tab and starting it again. Though it propts for saving and code generartion and closes successfully.
Solved! Go to Solution.
2023-04-18 06:23 AM
Hello @SeyyedMohammad
First thank you for posting and mentioning this behavior.
In fact this is an unexpected behavior and this problem is raised internally to be reviewed. I'll keep you posted with the updates. Internal ticket number: 150036 (This is an internal tracking number and is not accessible or usable by customers).
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-17 10:21 AM
Hello @SeyyedMohammad,
Could you please precise the CubeMx version used? If possible to share the ioc file.
I will let our CubeMx expert @Semer CHERNI investigate more this issue.
Imen
2023-04-17 11:29 PM - edited 2023-11-20 07:57 AM
Hi! @Imen DAHMEN
I think it can be happens on every project, when you are in project and switching between peripherals sometime clicking on MDMA causes not responding. And the CubeMx version is what included in the cubeIDE 1.12. ioc added.
Thank you so miuch. Also clicking on the system view dissapering arrow will causes:
Thnk you so much for your attendant.
2023-04-18 06:23 AM
Hello @SeyyedMohammad
First thank you for posting and mentioning this behavior.
In fact this is an unexpected behavior and this problem is raised internally to be reviewed. I'll keep you posted with the updates. Internal ticket number: 150036 (This is an internal tracking number and is not accessible or usable by customers).
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.